AXIS#.IL.LIMITP

Description

This parameter sets the positive user limit clamp value of the torque-producing q-component current command (AXIS#.IL.CMD ). The current command is additionally limited by the motor peak current setting (AXIS#.MOTOR.IPEAK ) and by the present value of the foldback I²t peak motor current protection.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

A

Range

0 A to drive peak current (IPEAK)

Default Value

Drive peak current (IPEAK)

Data Type

Float

See Also

AXIS#.IL.LIMITN
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
AXIS1.IL.LIMITP

500ah

04h

Signed32

-

1000:1

Read/Write

No

AXIS2.IL.LIMITP

510ah

04h

Signed32

-

1000:1

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.IL.LIMITP

5814

16B6

Signed32

Read/Write

-

AXIS2.IL.LIMITP

71350

116B

Signed32

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.IL.LIMITP

5814

Float

Read/Write

-